atvracer (Customer) asked a question.
productivty with sure servo
i just ordered another p1-550 and a sure servo setup. my question is what is the bestway to link these 2 up? modbus or direct I/O or ?? i have never used modbus. my setup it will need accel and decel controls and adjustable pos and feed rate controlled with a HMI. at the end i will have 6 of these machines interfacing with 3 Fanuc robots i got the IP/ethernet link worked out on that end
thanks
the P1 series currently does not have a high speed output card so i would probably go with modbus. I have used the PWM card to accel and decel a stepper motor but am not doing any position control with it.
ok so if i was to use p2 with a high speed card that would be a better option ?
thanks
I wouldn't necessarily say better but the programming would be easier as you could take advantage of the high speed I/O instructions in the productivity suite.
cool that helps a lot
thanks
If you do use a P1k with servo and want to be able to dynamically select a position from an HMI input then your only option is modbus with the servo in position mode. You would have to communicate the number of revolutions and partial counts of a revolution into one of the position commands and then execute that command.
If you were to use digital IO, you can pre-set something like 6 or 8 positions in the servo drive and then select a move to those positions with your digital inputs, however you cannot change where those pre-set positions are without either manually entering the data by hand on the drive unit or communicating new data for a position via modbus.
P2k with a high speed output card is much easier to configure and do a move on, as you can handle all of it in the productivity program. Simply assign your target position to a floatingpoint32 tag, and then write any value you want to that from your HMI. As long as you actually did your hardware set up properly it will all work easily.
It could be done either method though.
Also, determine how you are going to zero the drive positions. I run the servos in torque mode and run the actuator up against a hard stop. The PLC requires a user acknowledgement and the system zeros. I am not an expert in motion control or even PLC programming, but with a little reading and testing, I got it all working and have very little issues. One glitch I did discover is the MODBUS interlocking to prevent communication conflicts. This is outlined in some sample projects (I cannot remember where on this site). Got that straightened out and no issues since.
thanks for your replays i got a 2000 playing with it in between my other projects got a question one of my
servos setups i have a press with a geared servo and want to adjust the speed at precisely at certain spots but without stopping the press just adjust the speed with a S curve accelerate and decelerate to allow the press slow down load apart then speed up top full speed to feed par and still be able to stop the press at a precise spot when running in single part mode and no stop in auto mode
thanks
Over modbus, in addition to position, servo speed can be sent with each move command. In fact, almost any setting in the servo can be adjusted over modbus.
For your press, you could issue a position command, (over modbus), while continuously monitoring actual position, and in the ladder, when the position reaches your predetermined setpoint, change the speed over modbus.
thanks Dave
ill give this a try