Glen_Walker (Customer) asked a question.

Retentive Tags

Does anyone use Retentive Tags on their applications? Im looking at having several internal tags that the Operator uses for Email Addresses, and Batching Descriptions. My question is Can these tags be saved with the Application (The Contents of the Tag) and uploaded or saved so that if we do a download it will not erase the contents of these tags


  • ADC_HMI_PE (AutomationDirect)

    Retentive Tags are only retentive in case of power loss. They are backed up in memory by a Super Capacitor.

     

    One option is to use the Call Recipe button with a Recipe Sheet. You can insert rows and read the current values into a row in the Recipe Sheet. These become part of the project when it is backed up or read from the panel. But will be overwritten if the original project is written in to the panel.

     

    The one caveat is that these must be PLC tags. This will not work with Internal Tags.

    Expand Post