gmweber (Customer) asked a question.
Alarm Banner covers over canned screens in CM5 v9
On all previous versions of C-More software, the canned software screens such as the Alarm screen and Recipe screen ignored any active alarm banner. On the new CM5 version, the alarm banner and error banner appear to cover over these screens. This is a problem if left on the default setting of the bottom of the screen, as it covers up all buttons that are fixed to that location on both of these screens. I can move it to the top, but then you lose any label or header as well.
Any idea why this change was made? Is there a way around this issue?