ADC Community_02 (Automationdirect.com) asked a question.

Productivity Suite Software, Version 4.7.1.5

We are pleased to announce the release of Productivity Suite software, version 4.7.1.5

 

Improvements:

1. ST Editor: Added support for the long-form "TIME#" prefix for duration/time literals.

2. ST editor: Allows default display format for monitored values. 

 

Bug Fixes:

1. Fixed an issue where opening a project could hang the software, requiring a force close.

2. Corrected a defect where the Ladder Editor could hang or freeze while in debug mode.

3. ST Editor: Added a validation error when a constant array index is out of bounds in the ST editor.

4. ST Editor: Addressed an issue where tags created in the ST editor weren't marked as 'In Use.'

5. ST Editor: Corrected where an undefined tag used only inside a subscript expression was incorrectly flagged as a syntax error.

6. ST Editor: Resolved a problem where an overflow check wasn't applied correctly for array paths within user-defined structures.

7. ST Editor: Addressed an issue where SLEN could return a value greater than 128 for string literals longer than 128 characters.

8. ST Editor: Fixed an issue where string equality comparisons always evaluated as true.

9. Resolved a problem where forcing a tag mapped to a UDI output parameter didn't work correctly.

10. Addressed an error when transferring a project with UDIs at runtime could trigger a '50000 Bytes Exceeded' error.

11. Corrected a defect when dragging a task with tags between software instances could silently fail.

12. Resolved a problem where some corrupted projects could compile with incorrect constant values in ladder logic.

13. Improved compile times for projects containing UDIs.

14. Fixed an issue where saving and compiling a project no longer simplified the ladder program.

15. Corrected the P1-M622-16DR controller displaying only 27K of available retentive memory instead of the correct amount.

16. Addressed an issue where Find/Replace didn't work with tags containing brackets.

17. Corrected where data logging stopped working when using scheduled data logging.

18. Fixed an issue preventing a power supply from being added to a P1-RX remote base.

19. Fixed an issue where removing default tags from IO modules prevented points from being reassigned.  

20. Fixed an issue where an invalid or undefined variable in a MATH instruction within a UDI could cause the CPU to lock up.

21. Resolve a problem of data not being log if a discrete tag being used as an event trigger. 

22. Corrected an issue where some variables are not being found in search/replace with a ST task in project.

23. Fixed an issue where Px-622 CPUs could not send email when the "Add Saved File" option was selected.

 

Go here to download the software