Todd Dice (Customer) asked a question.
I was at a customer last week programming a P2-622 and could not get my laptop* to communicate over the USB-C connection. Does the connection require a specific cable? The cable I was attempting to use is the 10-foot version of THIS SET. Or could it be the driver didn't update properly? I ended up using a USB-A to Ethernet adapter and an Ethernet cable for the bottom connection to the CPU.
If the cable is at fault here, do you have a recommendation on a long cable? I need the cable long, as I never know exactly where a customer has their PLC mounted, and some have them in cabinets at the top of their equipment. Thanks!
*Edit: Dell, 64-bit running Windows 11.
@Todd Dice (Customer) Correction: the 622 series CPU connects as a network adapter, not via USB driver (see below). This uses NDIS (Network Driver Interface Specification), Microsoft's standard model linking network protocols to physical or virtual network hardware.
Note: some USB A-C cables are charge-only and won't work for communications. We recommend trying a different cable — we carry 6 ft. cables confirmed to work with all 622 series CPUs.