Jerred (Customer) asked a question.

[Fixed?] [Error] Wrong number of IO tags for module at group 1 base 1 slot 1
Psuite 4.7.0 (47)

I'm not sure if anyone has come across this with their programs. I ran into this error when working on some updates on an automated cell. I found that my P2-16ND3-1 was only showing 15 inputs, I am not sure how this happened as the program has been running and is still running without issue. I was able to drag and drop a P2-16ND3-1 on the hardware configuration screen, and it refreshed the card to have the 16th input. Seems to be working so far. I just wanted to put this here in case someone else runs into a similar issue.

 

P2-16ND3-1 missing input


  • ADC Community_02 (Automationdirect.com)

    This is a known issue and has been fixed in the next maintenance release of the software.

    Selected as Best