AFK33 (Customer) asked a question.

GS20 Drive Read but not Writing with GS20A-CM-ENETIP Card

I have a GS23-55PO1 with a GS20A-CM-ENETIP comms card connected to a productivity 2000 PLC. I have set the parameters on the drive to communicate using the adapter card and can get a read success. The write function says 'No Parameters" when it is off and "slave device fa" when it is triggered on. I have used this same set up in another project and had no problems. This PLC runs several other motors but using Modbus comms. I have replaced the comms card and still no results. For reference i do have a polling offset from the read and the write command. Any advice would be appreciated, ThanksWith AutoRun ONWith Auto Run OFF.


  • AFK33 (Customer)

    Thank you for the help. I had it set to 1 as per the instructions in appendix B: Optional I/O Communications Cards of the GS Drive Manual.