ADC Community_02 (Automationdirect.com) asked a question.
We are pleased to announce the release of Productivity Suite software, version 4.7.0.47
Improvements:
1. Added Structured Text support, enabling users to create powerful expressions and structured logic using statements and operators, based on — but not identical to — IEC 61131-3 standards.
2. Added a UDI Library for storing User Defined Instruction definitions, allowing definitions to be reused across multiple projects.
3. Added a new Delta Contact that triggers when the previous scan value does not equal the current scan value.
4. Added support for new modules: P2-08ADS-1, P2-08ADS-2, P2-15CDD1, P2-15CDD2, P2-16CDR, and P2-16TEP.
5. Added support to allow up to (8) P2-RS to operate with a P3-622.
6. Added the ability to save tag values, allowing users to upload and download values for selected data types.
7. Added the option to include tags in exported TagDB.
8. Added UDI support in the Find/Replace feature.
9. EDS: Added support for Read-Only Parameters within Assemblies.
10. EDS: Added support for Non-Displayed Parameters within Assemblies.
11. EDS: Added support for Array keyword entries when importing EDS files.
12. Added a CPU Logout option via CPU → Logout of CPU.
13. Added a modified indicator for tasks that have changed since the last save or sync, consistent with existing rung-level indicators.
14. The Delete key now removes selected tag(s) from the TagDB.
15. The Insert key in Dataview now opens a dialog to add new row(s).
Bug Fixes:
1. Fixed an issue where the FIFO instruction's Clear operation returned a NULL value.
2. Reduced the performance impact of Version Control status updates.
3. New Gen: Fixed a Modbus Structure issue where the quantity of registers did not match the number of bytes.
4. Fixed an issue preventing task creation in the Task Library.
5. Fixed an issue where some projects failed to transfer when using the Simulator.
6. Improved error handling for cases where the software became stuck on the splash screen.
7. Fixed an issue where the P3-622 File Systems widget incorrectly displayed MicroSD.
8. Fixed an issue where task folders containing tasks with UDIs could not be dragged to a different location.
9. Fixed an issue where deleting a local tag assigned to a ladder instruction left the instruction without a tag, but the UDI instance continued to compile and run.
10. Fixed an issue where creating a tag instance of a UDI structure used an incorrect data type when the UDI contained a system structure parameter with non-standard data types.
11. Fixed an issue where array tags were not being retained after saving a project for Network Read (RX/WX) and NETW instructions.
12. Px-622: Fixed an issue where the Modbus TCP server on port 502 would stop responding after repeated TCP connection attempts.
13. Px-622: Resolved an issue where transferring a project over VPN could intermittently cause the CPU to enter a boot loop.
14. Resolved an issue where moving tasks or folders could cause task folders to appear missing or duplicated.
15. Px-622: Fixed an issue where sending an email to 4 or more recipients triggered an invalid address error.
Go here to download the software