hfiles (Customer) asked a question.
I have a device that I was previously able to scan for and connect to via codesys. I was troubleshooting an issue with my project not being able to download without a codementer error when there was a visualization in my project and got to a point, I was looking at the certificates in the device to see if that could be an issue. I shut down my device for the day after not finding a solution to that error then could not scan for the device the next day.
I am able to ping the device from command prompt, but I am unable to scan for it in my codesys project. I tried to see if I could wipe the project out of the system, but the P2CDS firmware project could not see the device either.
I have also tried setting the adjust ethernet settings parameter in the NetConfig window of the codesys project back to true and tried to reconnect with the USB connection without progress.
The USB connection does show up in the device manager.
I'm looking to see if it show up in Windows Network Connections.
You can type in to the windows search bar network and you should see the option View network connections. It will be a unidentified network and the device would be a remote NDIS Network Device.
If it is there you can try the following:
If this doesn't work then I would continue with the replacement. My apologies for the issues you're experiencing.