PouchesInc (Customer) asked a question.
Im not sure how far back this goes or if this is only a problem on the latest Productivity version available for download. Just looked and it is running V4.6.2.2
When I have the Tag Database window open on the main screen it functions fine and I can create new tags. When I press the Add Tag button a new window opens.
If the Tag Database window is on a secondary screen however, pressing Add Tag causes the program to freeze. No window opens and Productivity is unresponsive.
I have attempted this multiple times with the same behavior each time and between reboots, and verified the window position on either screen does not matter. I must open Task manager and force kill the program to close it and then I can reopen the program fine.
I have taken two screenshots showing one where the window opens fine and another where the program is locked up, as well as made a short video showing one of the tests I did. In the video you can see the button actually press in the first time I click on it while on the secondary screen, and then all future clicks do not do anything and just produce an error sound in Windows
System is an Asus laptop running Windows 11 Pro v25H2.
Video link since it is too large to upload:
https://drive.google.com/file/d/1XA-ljCCizgUDICmatgZX8RTkBQKu2ogL/view?usp=sharing
I was unable to reproduce the issue you reported in version 4.6.2.2. If you'd like to share your project via private message, I'd be happy to investigate further on my end.