willpoll (Customer) asked a question.
Anyone else experiencing CM5 Safe Mode issues when no update is being performed?
I've have 3 CM5-T10W go into safe mode while deployed, with no updates being performed.

willpoll (Customer) asked a question.
Anyone else experiencing CM5 Safe Mode issues when no update is being performed?
I've have 3 CM5-T10W go into safe mode while deployed, with no updates being performed.

Well, they have no firmware right now :-( But, I believe they were on 8.21.
Try updating the firmware to v8.26. If the update goes smoothly test them to see if it occurs again.
How long does it usually take for them to go into safe mode after they are online?

They don't go online, they're stuck in safe mode. I've attempted to load 8.26, they sit in 'loading program' for at least 20 minutes.
Thanks,
I found your active support case and discussed it with the technician over that case. He should be emailing you from the support case as soon as he can.

I downloaded 9.00 and was able to fix both with the 9.00 firmware, then I was able to roll both back successfully to 8.26.
These were originally 8.10 and 8.11 when they entered safe mode.
Thank you for letting us know. If you can connect in safe mode a firmware update is an option.

This issue has been addressed in V8.27 and V9.02 depending on which you use in your system. The latest firmware is available on our downloads site at:
https://www.automationdirect.com/support/software-downloads?itemcode=C-more%20CM5%20Series#
Copyright © 1999-2023 AutomationDirect. ALL RIGHTS RESERVED
Thank you for letting us know. If you can connect in safe mode a firmware update is an option.