NatTebb (Customer) asked a question.

P1AM Analog Input Precision

My team is trying to make a system with this PLC to track 2-3 analog inputs at 200hz. We recently learned the P1-4ADL2DAL-2 was never going to be able to keep up with that, so we're thinking about using the A0-A5 inputs on the side of the center module. But those inputs can only take 3.3V, our analog sensors run on 12V. We're willing to use voltage dividers to drop the voltage, but obviously we're now concerned if the P1AM will able to be able to read those sensors with the same precision AND range a 12v setup would be able to.

 

Also to be clear im a junior member of the team, so if something seems weird, please ask before castigating.