Bar (Customer) asked a question.

Flasher instruction doesn't seem to work on Do-more

Hello,

I am having trouble using the flasher instruction. I would like the output bit C6 to turn on and off. Both contacts are true, but C6 does not come on. Any ideas on why this would be?

Thanks

Image showing Flasher circuit.


  • HOST_franji1 (HOST Engineering)

    Look at the Cross Reference for C6 and see if something else is writing to it - Expand Ranges to see if there is any RSTR or casts or whatever possibly writing to C6. Find All C6 in the Find dialog may also be helpful (do NOT check "Exact").

     

    Is the logic in a code block that is NOT running? Or is the rung in a Stage that is inactive? Expand the Project Browser Control Logic node to that code block and Stage and turn Status ON on the Project Browser toolbar to get details on the running and stage state info.

    Expand Post
    Selected as Best
  • HOST_franji1 (HOST Engineering)

    Look at the Cross Reference for C6 and see if something else is writing to it - Expand Ranges to see if there is any RSTR or casts or whatever possibly writing to C6. Find All C6 in the Find dialog may also be helpful (do NOT check "Exact").

     

    Is the logic in a code block that is NOT running? Or is the rung in a Stage that is inactive? Expand the Project Browser Control Logic node to that code block and Stage and turn Status ON on the Project Browser toolbar to get details on the running and stage state info.

    Expand Post
    Selected as Best
    • Bar (Customer)

      I ended up taking this out of the ladder diagram.