Dagear (Customer) asked a question.
PS-AMC Registration, Positive and Negative limits
First application with PS-AMC1, I have a Teknic's SDSK motor connected to the PS-AMC via a signal conditioner as the outputs from the PS-AMC1 are low level and Teknic requires higher voltages. I can get scaling, and motion to occur, but even though I see the limit inputs 4 & 5 change state, pulses continue to get sent to the motor, eventually running it into a hard stop.
I've been discussing with Wayne via E-mail, but thought I would post here to see if other have experienced the same issue.
Couple thoughts I'm going to try
- Aux 24 VDC is not connected and system is working, going to connect this up and see if has something to do with the internal pull up resistors.
- may roll back or look for a firmware match for controller & PSAMC
- Connect the drive through the Enable output to see if the limits drop the enable.