EIglesias (Customer) asked a question.
SPI Pin Conflicts and Integration Challenges with P1AM-100, P1AM-Serial, P1AM-Eth, P1-04TRS, and MKR CAN Shield
I’m currently working on a project using the P1AM-100 along with several expansion modules:
- MKR CAN Shield
- P1AM-Serial
- P1AM-Eth
- P1-04TRS
I’m running into some issues related to SPI pin conflicts and integrating all the modules together. I’m hoping to get some guidance from anyone who has done a similar multi-shield setup.
SPI pin assignments:
- CAN_CS_PIN = 4, INT = 7, SCK = 9, MOSI = 8, MISO = 10
- ETH_CS_PIN = 5, SCK = 9, MOSI = 8, MISO = 10
- Serial_Port1: RS232/485Sel = 3, RX = 13, Tx = 14, RS485 DE/RE = A6
- Serial_Port2: RS232/485Sel = 2, RX = 1, Tx = 0, RS485 DE/RE = 6
- Base_Controller: CS = A3, ACK = A4, SCK = 9, MOSI = 8, MISO = 10
Integration complexity:
- Getting CAN, Ethernet (Modbus TCP), and RS485 (Modbus RTU) all running reliably on the same board has been tricky.
Questions for the community:
- Are there best practices for combining P1AM modules with MKR CAN Shield?
- Any tips for avoiding SPI conflicts or managing multiple SPI devices with the P1AM-100?
- Any recommended workflow for integrating Modbus TCP + Modbus RTU + CAN on a single P1AM setup?
Any insight or guidance would be greatly appreciated!
Hey @EIglesias (Customer) ,
I want to double check you're using the official Arduino MKR CAN shield - if so I believe the CS pin is actually 3 and not 4. Unfortunately this does create a conflict with the P1AM-SERIAL that could be an issue if you're running an RTU Server as toggling the CAN CS would change from 232-485 mode. There is the possibility of modifying the hardware/library of the MKR CAN shield by cutting the pin trace on 3 and jumpering it to 4 in addition to altering the code to reflect this change.
For general advice on getting all of these running together I would recommend
Thanks
Adam