ThatShouldHaveWorked (Customer) asked a question.
I have a servo amplifier that sat a bit to long on the shelf. The OEM procedure to reform the caps is by reducing the line voltage and then dwell and step up over a period of hours.
In theory I should be able to use a frequency drive to do it. Set max output voltage to % then run it a 60HZ.
Has anyone used a drive this way?
My OPINION is do not use a VFD for this..
A VFD does not actually reduce Voltage to the 'Motor' it Just reduces time 'On' and lets the Pulse Charge the Magnetic Strength of the Coil in the Motor, simulating a low voltage run condition..
You are charging a Capacitor, and when you hit it with a Peek of ( Say ) 600 VDC, no matter how long, it might complain..
I like the Variac Method..
Cap