Ap12 (Customer) asked a question.
we are using windows pc ,so is there any ref lib or python app available to control the driver and is there any recommended converters/connectors preferred for smooth operation since we have only one driver will be connected Modbus protocol is required ?
our ref python app
import minimalmodbus
import serial
import time
def test_sureservo2():
try:
# CORRECTED: SureServo2 specific settings
servo = minimalmodbus.Instrument('COM4', 127) # Slave 127 (not 1!)
servo.serial.baudrate = 9600 # 9600 baud (not 115200!)
servo.serial.bytesize = 8
servo.serial.parity = serial.PARITY_NONE
servo.serial.stopbits = 1 # 1 stop bit (not 2!)
servo.serial.timeout = 2.0 # 2 second timeout
servo.mode = minimalmodbus.MODE_RTU
print(" SureServo2 Control Test - CORRECTED VERSION")
print("=" * 50)
# Test 1: Read firmware version P0.000 (register 0x0001)
print("Reading firmware version...")
fw = servo.read_registers(0x0001, 2, functioncode=3)
firmware_value = (fw[0] << 16) + fw[1]
print(f"Firmware version: {firmware_value} (0x{firmware_value:08X})")
print(f" Raw registers: {fw}")
time.sleep(1)
# Test 2: Read current alarm P0.001 (register 0x0002)
print("\n Checking for alarms...")
alarm = servo.read_registers(0x0002, 2, functioncode=3)
alarm_value = (alarm[0] << 16) + alarm[1]
if alarm_value == 0:
print("No alarms - Drive ready")
else:
print(f"Alarm code: {alarm_value}")
time.sleep(1)
# Test 3: Enable servo P2.030 (register 0x021F)
print("\n Enabling servo...")
servo.write_long(0x021F, 1, functioncode=16) # CORRECTED address
print(" Servo enable command sent")
time.sleep(2)
# Test 4: Set position register P5.001 (register 0x1389)
print("\n Setting target position...")
servo.write_long(0x1389, 1800, functioncode=16) # CORRECTED address
print("Position set to 1800 pulses")
time.sleep(1)
# Test 5: Execute position register P5.007 (register 0x138F)
print("\n Executing movement...")
servo.write_long(0x138F, 1, functioncode=16) # CORRECTED address
print("Movement command sent - Motor should move!")
time.sleep(3)
# Test 6: Stop/disable servo
print("\n Stopping servo...")
servo.write_long(0x021F, 0, functioncode=16) # Disable servo
print(" Servo disabled")
print("\n All tests completed successfully!")
except Exception as e:
print(f"\n Error: {e}")
print("\nTroubleshooting:")
print("1. Check SureServo2 is powered ON")
print("2. Verify wiring: Blue→D+, White/Blue→D-")
print("3. Make sure no AL.xxx errors on display")
print("4. Try swapping D+ and D- wires if needed")
if __name__ == "__main__":
# Install minimalmodbus first: pip install minimalmodbus
test_sureservo2()