Nikiolas_bb (Customer) asked a question.

symbol configuration. Waintek cmt2078x panel

Hello,

 

This is the errors I am getting below for the symbol configuration.

How to fix this (Waintek cmt2078x panel )

 

 

 

        ------ Build started: Application: Device.Application -------

        Typify code...

[ERROR]     iecvaraccess, 4.2.0.0 (system): Initialize [IecVarAccess]: C0032: Cannot convert type 'Unknown type: 'IecVarAccRegisterInstance3(_IIecVarAccess3, ADR(result))'' to type 'POINTER TO BYTE'

[ERROR]     iecvaraccess, 4.2.0.0 (system): Initialize [IecVarAccess]: C0046: Identifier 'IecVarAccRegisterInstance3' not defined

[ERROR]     iecvaraccess, 4.2.0.0 (system): Initialize [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccRegisterInstance3'

[ERROR]     iecvaraccess, 4.2.0.0 (system): FB_Exit [IecVarAccess]: C0046: Identifier 'IecVarAccUnregisterInstance' not defined

[ERROR]     iecvaraccess, 4.2.0.0 (system): FB_Exit [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccUnregisterInstance'

        Compile complete -- 5 errors, 0 warnings

 

 

 


  • FACTS_MikeSc (AutomationDirect)

    The P2CDS-622 currently does not support symbol configuration.

     

    I'm not familiar with using these HMI's but after a little researching it looks like you can talk to these over modbus which the P2CDS-622 supports.

     

    If you have more questions feel free to ask to see if we can offer some help.

  • Durallymax (Customer)

    Well that's a bummer, symbol config gives you full symbolic support in EBPro and none of the Modbus hassles.