JB2020 (Customer) asked a question.

Werma IO Link Stack Light Communications

In conjunction with my IO Link Durability post... I have decided to go with remote IO bases for all of my field IO. However, I want to use one of Wermas 15 Tier StackLights for my main panel. I don't want to buy an 8 port IO Link master for 1 IO Link device. Are there 1 port or 2 port masters for such a situation that work with Productivity? Or is there another option altogether?


  • Bolt (Customer)

    Your options are fairly limited, there are no single port masters available. I don't know of any modbus/ethernet/etc stack lights that come close to the 15 tiers. You can program the Wermas to 64 pre-configured patterns, and use 6 digital outputs from your PLC to select those 64 patterns.

  • Durallymax (Customer)

    There's nothing inherently special about working with Productivity, find one that speaks Modbus TCP or EIP and it will work. The IFM 1 port master is for USB config only and the 2 port is AS-i.

     

    As mentioned, depending on how many unique patterns you need, you can also just program the discrete version of the light via USB and output whatever pattern you want over 1-6 discrete outputs.

    Expand Post