NativeFunction (Customer) asked a question.
I have a P2CDS-622 on CODESYS V3.5 SP20 Patch 5 and I follow what is defined here https://docs.codesys-p2cds622.com/en/latest/Additional%20Topics/coincell_volt.html
In order to read byBatteryIsVoltageTooLow but when I add the device codesys states "[ERROR] 485v2: P2CDS622_SystemTags [Device]: C0046: Identifier 'IoDrvP2cds622SystemTags.IoDrvP2cds622SystemTagsDiag' not defined". This error originates from the P2CDS622_SystemTags device -> Internal IEC Objects -> Type. The IoDrvP2cds622SystemTags library is added in library manager but i don't see where IoDrvP2cds622SystemTagsDiag is in the lib. Is the P2CDS622_SystemTags device broken in the current version of the P2CDS-622 Package v1.0.0.4?
Working on my end with the latest "P2CDS622" Device at 1.1.10.0
Inserted:
Removed:
?- would you send the screenshot of the following Device > PLC Settings: