NNZ (Customer) asked a question.
LS XGB (XEM DP32H2) to CM5 T10W
Wondering if anyone has setup one of the CM5 series of HMI's with the LS XGB series of PLC's? The HMI does not have the PLC protocol for the LS XGB PLC's and I was wondering what the best options would be for getting them to communicate. I was planning on doing it through serial communications, but Ethernet IP is fine as well.
ModBus TCP or ModBus RTU would be the best options.
Our interactive help site for ModBus TCP to CM5 is at https://cdn.automationdirect.com/static/helpfiles/ls_plc/Content/C_ProcedureTopics/LP203-1.htm?tocpath=%20Procedures%7CCommunications%7CConnect%20to%20C-More%7C_____1