jdjennings1962 (Customer) asked a question.
Can anyone give me suggestions for finding the source of an unexpected delay?
I have the P2CDS-622 with P2-8AD4DA-1 analog card. I wired AO0 directly to AI0 with a very simple program. Program cycle time set to 3 mS. AI on COURSE setting. Using high speed TRACE set to follow main program cycle time. Plotting the raw integer without filter, seeing 3mS resolution on trace. I am observing a delay of > 100 mS on trace to detect step change. With WAGO PLC in similar settings, I observe 26 mS delay. But specs of P2-8AD4DA-1 card appear better than specs of WAGO (single digit mS on AO/AI in Course mode).
Thank you
Yes that is too long, not sure if its related to CSYS and the Trace utility program overhead.
The real reference is if you can scope it and see actual H/W performance. From writing the variable for the channel to the output changing on the scope. Dont mean to state the obvious, but just trying to get some data on this. That number should be less than 20ms for sure in Coarse mode.