ADC_HmiClicK_PE01 (AutomationDirect) asked a question.
CLICK 3.60 with support for Remote PLC Mobile App
CLICK 3.60 and a new mobile app called Remote PLC are now available. The CLICK software can be found at the software downloads page.
Remote PLC can be found on the Apple app store: For Android users, it can also be found on the Google Play Store:
We would love to hear your thoughts on this latest release!
Thank you for having the selection of the "classic menu" when installing the software. I do prefer having all the tools on one page.
Links
Play Store
Apple
Software seems fine. Updating firmware C2-01CPU keeps crashing
How are you connected to the CPU? USB, or Ethernet? Is there wifi, or a switch involved? It's probably best to contact support and have someone look at this with you.
"There's a known issue with 169.254.x.x addresses causing this type of problem on FW updates. 169.254.x.x. addresses are special reserved in the ethernet standards and are problematic.
If you highlight the plc in the connect window and click on Edit below the list you can change the plc's address to something non-reserved like 192.168.1.10. After that you may need to adjust your pc's ethernet address to 192.168.1.100 (it can be 192.168.1.anything except 10)"
That was the issue and solution to the problem I was having. The above message was from ADC Technical Experience Team.