Ryan Poethke (Customer) asked a question.

C-more EA-9 setting MIN and MAX values for numeric entry

Software v.6.75. I have a C-more EA9 panel, with a numeric entry object. It's referencing an unsigned 32bit INT.

 

Have I lost my mind, or did there used to be a way to set MIN and MAX values so an operator couldn't enter numbers outside a range? I know I can do it on a C-more Micro and I though I've done it before on the EA9. I've looked through all the option tabs for the object, and I don't see MIN and MAX anywhere.

 

 

Thanks,

 

Ryan Poethke


  • Durallymax (Customer)

    Check the mark for range and you can enter it there but these are fixed values and not a tag so in some cases it's easier/beneficial to clamp in PLC instead.

  • kewakl (Customer)

    Request: Make these fields tagable

    • ADC_HMI_PE (AutomationDirect)

      We definitely have that on the short list.

      • Les67 (Customer)

        A real short list please.