Pa (Customer) asked a question.

Can the Rhino DC-DC converters have the 0V tied together?

I have a project where I need to use the PSP24-DC12-1 to get from 12V to 24V to run a CLICK PLC, and it would really help if I could tie the 0V from both sides together. I know sometimes you can but I want to make sure so it doesn't burn out down the road.