Reer Mosaic Safety Controllers Software release V1.9.0.2

https://www.automationdirect.com/support/software-downloads?itemcode=MOSAIC%20Safety%20Designer

 

What's new: 

 

1) Configuration:when the Bus module is inserted, the module image changes according to the chosen specialization

2) Single-Double OSSD: when these outputs are configured with Reset, the Reset Pin to be used can be reallocated on any of those available.

In addition, multiple outputs with active Reset can share the same Reset

3) The unused Restart/Fbk Pins can be used as single inputs in the schematic

4) Speed items: the terminal shows the real name of the module instead of the generic name MV1/MV2

5) The project report changes: it is now available either in HTML or PDF format with renewed graphics

6) Network Operator adds a new Output Pin: Request. This Output is the Reset request

7) Upload Process: at the end, the source file is compressed and transferred to the Master module. When downloading a project, if the msx

source file is stored on Master it will be totally recovered including its original name

8) System Command: there is a new button Create configuration that allows creating a new configuration starting from the recognized

modules list

9)Table Monitor: used a new structured table with a Tab for each module

10) Bugs fixed: Minor bug fixed


  • ADC Community_02 (Automationdirect.com)

    Reer Mosaic Safety Controllers Software release V1.9.0.2