SdG313 (Customer) asked a question.
Hello,
I have a complex PLC program in which the previous programmer has defined many variables as INT data type when BOOL would have sufficed. A value of 0 or 1 is written to the INT variable. Different brands of HMI can set up a push button to trigger just one particular bit of the INT data type or write an integer value of 0 using a push button. Couldn't find an obvious way to do this on C-more unless I am missing something.
I would like to avoid altering the PLC code just because of how complex it is and will require too much time. Hopefully there is an easier solution directly through C-more
Which cmore model / sw rev?
EA9 has this construct: