Linuxdept (Customer) asked a question.
Working with a P2-02HSC
Working with a P2-02HSC and Connecting to a Encoder , Does anyone have any Examples of Ladder for the Productivity 2000 for working with this card ...
Linuxdept (Customer) asked a question.
Working with a P2-02HSC and Connecting to a Encoder , Does anyone have any Examples of Ladder for the Productivity 2000 for working with this card ...
Copyright © 1999-2023 AutomationDirect. ALL RIGHTS RESERVED
We do have one example:
https://community.automationdirect.com/s/article/PROGRAMMING-EMAMPLE-Productivity-Series-HSC-rate-calculation
Maybe it is just me, but the forum says I cant access the link you posted.
Could be an issue with our Vendor of the community. I have attached a copy of the example until issue is resolved.
_________________________________________________________
Title:
PROGRAMMING EMAMPLE: Productivity Series: Px-02HSC rate calculation
Details:
Reference the attached .adpro ladder example that uses the "CHANGE OF VALUE" instruction to calculate the rate of the pulse count coming into the Px-02HSC.
Note: Project written using version Productivity Suite 3.7.x.x
HSC Sample Rate Example
@PouchesInc (Customer) The issue of accessing the knowledge article should be fixed. Can you click on the below link again and see if the issue is resolved?
https://community.automationdirect.com/s/article/PROGRAMMING-EMAMPLE-Productivity-Series-HSC-rate-calculation
I can access the link.
Garry
Yes, it works now. Thank you.
ok. now switching Gears here. but what about the P2-HSI can i get examples on that as well , here is what we done with the Click in the past.i need to make this into Productivity using the P2-HSI