Heriberto (Customer) asked a question.

Hello. Can you help me, please? I need to increase the dimensions messages box alarm. The windows that display in alarms are very small and the customer need bigger.


  • Garry (Customer)

    You are correct, I was looking at the popup window frame. You have the event message box. There is no way to increase this size that I can see.

    Regards,

    Garry

    Selected as Best
  • Durallymax (Customer)

    Are you referring to the alarm list or the alarm banner?

     

    The banner size can be changed in the panel manager.

    PanelManagerBanne 

    The alarm list row height can be increased by changing the text size.

     

    AlarmListCMore

    Expand Post
  • Heriberto (Customer)

    Thank you @Durallymax (Customer)​ . Im sorry, Im not explaining correctly. Im referring to next example:EXAMPLE_MESSAGE_ALARM

      • Heriberto (Customer)

        Hi @Garry (Customer)​ ,

        This display looks like has been windows 10 but it is part of HMI EA9-T7CL. The popup in the example is displayed when a alarm is activated. I will explain the example image I sent: when the alarm "no there foam" this pop-up (in the circle red) displayed "fill foam to the boxes". All this in the HMI. If I don´t explain correctly, please let me know. Thank you again!

        Expand Post
      • Garry (Customer)

        Hi @Heriberto (Customer)​,

        You explained it perfectly. Double click on the popup window frame to bring up the properties.

        EA9 Popup SizeThe display screen will show you what page the information is coming from. In my case, this is page 2.

        Go to the page and modify the size of the information. You will then have to go back to the page that has the information and change the container size to match the larger objects.

        Regards,

        Garry

         

        Expand Post
      • Heriberto (Customer)

        Thank you very much @Garry (Customer)​ !!! I will do tests.

      • Heriberto (Customer)

        Sorry @Garry (Customer)​ . I think the popup you used as an example is of another type. In the following image you can see the pop-up windows that I use, which are the ones that I need to modify. Unless I have understood you.EXAMPLE_MESSAGE_ALARM_2

      • Garry (Customer)

        You are correct, I was looking at the popup window frame. You have the event message box. There is no way to increase this size that I can see.

        Regards,

        Garry

        Selected as Best
      • Heriberto (Customer)

        All right, @Garry (Customer)​ . Again, thank you very much for your feedback.

10 of 11