martinav (Customer) asked a question.
I'm not quite following this. Ive watched a few videos, but they connect to an on/off device like a relay. I want to connec this to measure distance to an object. A bit different scenario. I assume I'm going to use the "W" block on my BX-DM1E-18ER3, but I'm not sure how it goes.
I see this diagram, but I'm not getting what is what.
Device is a DW-AD-509-M18-320.
Hi martinav,
Connect only the one analog input, not both. You will see that there is only one input, not two. WX0 is the input. WY0 is an analog output. Here is the wiring diagram for the current input.
When you open Do-More Designer you can then specify the signal coming on the analog input pin.
Regards,
Garry
https://accautomation.ca/series/brx-do-more-plc/