mashva (Customer) asked a question.
I'm using Prod Suite 3.8.0.14 and Windows 10.
1.) Hover over the Windows taskbar icon for Prod Suite until the thumbnail flyout appears
2.) Move your mouse to the flyout
3.) After a second, observe that all the open tasks should minimize except the task you are hovering over.
4.) Remember what this looks like.
5.) Add a rung into the ladder by right-clicking and select Insert > Rung > Before > OK
6.) Repeat steps 1-3
7.) What do you see?
Now, for as long as I have this instance of Prod Suite open, I will see this fake "Insert Rung Before" dialog any time I perform steps 1-3.
Once I actually give that task focus the dialog will disappear and I can continue to use the software without any issues but the dialog will show up that way every time until I close that instance.
It's only a little bothersome when I'm working with concurrent sessions of Prod Suite and I tend to use this method to switch between them.
Is this normal? Or is it something I've done?
I can duplicate. I tested all the way back to 3.0.0.31 and the issue still persists.
I can report this to our development team for review.
It's not a showstopper but its nice having some QoL fixes.
It's also nice to have a forum that is moderated well enough to respond so quickly!
Thanks!