rjm21 (Customer) asked a question.
Hoping someone has some experience with Fanuc Robots. Our company recently purchased a second hand Fanuc R-30iA Robot arm. Looking to add a C-More micro EA3-T4CL just to read certain values.
From the Fanuc manual: " HMI Device communication function. This function communicates with a HMI device by that the robot controller pretends to be a GE Fanuc Series 90 PLC."
This seems fine, as the C-More Micro HMI can communicate via SNPX protocol with GE Series 90 PLCs. And Google searches have turned up a couple of forum posts that the Robot does in fact do this.
What I'm most confused about is the wiring between the Robot and the C-More Micro. The serial port on the Robot is a special 20 pin port that is software selectable to communicate via RS-232C or RS422.
When using the SNPX protocol, will the C-More only accept RS-422, as indicated by the cable diagram? Or will it also accept RS2--232?
The reason I ask is the Pinout diagram for the Robot serial port doesn't list standard RS-422 pins such as RXD+, RXD-, TXD+,TXD-.
Pinout diagrams attached for reference. (Edited to upload higher quality version of the Fanuc Serial Pinout List)
To anyone in the future who may run into this, we had to purchase and install the HMI SNPX option from Fanuc Robots. Attached is the makeshift serial communications cable I had to make.