adccommunitymod (AutomationDirect) asked a question.
Kenetix 6000 Safe torque off code changes needed
Created Date: February 23,2015
Created By: bdkw1001
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am currently wiring in a MSR138.1DP Guardmaster safety relay to my Kenetix 6000 servo system. The rockwell rep said that I need to add some code to the PLC program. Was wondering if anyone out there has done this before and could steer me in the right direction. The rep said it is not much code to write. Thanks Ken
Created Date: February 25,2015
Created by: deep6ixed
We use the automation direct safety relay in our DC drive application, the only safety change we did in the PLC was to have the relay trigger a stop command, so that when the estop circuit was reset, the machine didn't take back off to full speed again.
The safety relay was tied into the Controlled Stop and Coasting stop signals. As soon as the relay opened the drive would power to a controlled stop. (Line draws wire through a die, has huge flywheel, so we have to use a powered stop) but after a set time (3 seconds) the timed contacts would open and remove power from the drive.
Created Date: February 25,2015
Created by: bdkw1001
Thanks
Thanks Deep6ixed, That Makes sense to tie it in with the stop command in the program. The relay I have does have the time delay, So I'll probably use this for the coast to stop that we need.
Thanks Again,
Ken
Created Date: February 23,2015
Created by: bdkw1001
I am currently wiring in a MSR138.1DP Guardmaster safety relay to my Kenetix 6000 servo system. The rockwell rep said that I need to add some code to the PLC program. Was wondering if anyone out there has done this before and could steer me in the right direction. The rep said it is not much code to write.
Thanks
Ken