adccommunitymod (AutomationDirect) asked a question.

sevvo motor use?

Created Date: February 19,2011

Created By: vf816

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I was wondering if any one here has used a AD servo motor for label application to round bottles at high speeds.I would like to use AD product to retrofit a existing label machine to apply pressure sensitive labels that are about 2.5x8 " in size.speeds at least 250 bbm.The labels come on rolls with 1/8 " gap between labels rolls weight is minimum less then 10lbs.I need to be able to set up for many different size labels. Any help is much appreciated Thanks in advance.


  • adccommunitymod (AutomationDirect)

    Created Date: February 19,2011

    Created by: vf816

    I was wondering if any one here has used a AD servo motor for label application to round bottles at high speeds.I would like to use AD product to retrofit a existing label machine to apply pressure sensitive labels that are about 2.5x8 " in size.speeds at least 250 bbm.The labels come on rolls with

    1/8 " gap between labels rolls weight is minimum less then 10lbs.I need to be able to set up for many different size labels.

    Any help is much appreciated

    Thanks in advance.

    Expand Post