adccommunitymod (AutomationDirect) asked a question.
Created Date: April 20,2007
Created By: a agnone
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Would anyone have a reason why a program running in a DL250-1 will not right correctly in a DL260? I can not find anything in the manual. Without getting into the specifics, it runs the homing sequence, then it will not run the positioning portion. I do a home of both axis using LD K10, then change modes with LD K20, that is when it just stops and will not run. If there is no real reason, I will have to dig deeper into the program. I am setting individual bits ex. B2056.0 etc.
Created Date: April 20,2007
Created by: a agnone
WHOOPS, I am using a CTRIO with the DL250-1, I loaded it into a DL260 and it does not work.
Created Date: April 20,2007
Created by: allukes
Do you have the latest firmware for the CTRIO module?
Created Date: April 21,2007
Created by: a agnone
I am checking.
Created Date: April 24,2007
Created by: a agnone
Do not forget to re-populate the v-memories when changing the CPU! Works just fine.
Created Date: April 24,2007
Created by: allukes
You might want to add the Vmemory Initialization at Power up, so you won't have the same problem again later.
Created Date: April 20,2007
Created by: a agnone
Would anyone have a reason why a program running in a DL250-1 will not right correctly in a DL260? I can not find anything in the manual. Without getting into the specifics, it runs the homing sequence, then it will not run the positioning portion. I do a home of both axis using LD K10, then change modes with LD K20, that is when it just stops and will not run. If there is no real reason, I will have to dig deeper into the program. I am setting individual bits ex. B2056.0 etc.