adccommunitymod (AutomationDirect) asked a question.

DL06 F0-08ADH-1 V-memory problem, values in memory not between 0 and 65535 . . .

Created Date: September 07,2016

Created By: steveola

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Greetings fellow travelers, I humbly climb the mountain to ask for the guru's help. :) I have a nice flat 11 mA going into my input card from a Vaisala HMM30C configured for 0-20 mA using the COM and CH5. (CH1 is working well at 16500 or so for another measured value.) I'm using an external Rhino power supply to drive the cards and the transmitters. I believe I have everything configured correctly: Input Card is in slot 1: LD/K800, OUT/V700, LDA/O3000, OUT/V701 I am washing it through the "smooting ladder, " LDD/V3010 (CH5,) BIN, BTOR, SUBR/V3704 . . . etc. My other channels are unoccupied at the moment, here is what I get: n102590 Any ideas where that overflow is coming from? I almost hesitate to ask, I know it is going to be simple. :) Do I have to use the on board power supply to drive the cards? Many thanks, Steve


  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2016

    Created by: steveola

    Greetings fellow travelers, I humbly climb the mountain to ask for the guru's help. :)

    I have a nice flat 11 mA going into my input card from a Vaisala HMM30C configured for 0-20 mA using the COM and CH5. (CH1 is working well at 16500 or so for another measured value.)

    I'm using an external Rhino power supply to drive the cards and the transmitters.

    I believe I have everything configured correctly:

    Input Card is in slot 1: LD/K800, OUT/V700, LDA/O3000, OUT/V701

    I am washing it through the "smooting ladder, " LDD/V3010 (CH5,) BIN, BTOR, SUBR/V3704 . . . etc.

    My other channels are unoccupied at the moment, here is what I get:

    n102590

    Any ideas where that overflow is coming from? I almost hesitate to ask, I know it is going to be simple. :)

    Do I have to use the on board power supply to drive the cards?

    Many thanks,

    Steve

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2016

    Created by: steveola

    PS . . . I did a search of the ladder for V3010 and the only instance of V3010 (or by extension V3011) is the first line of the smoothing rung.

  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2016

    Created by: mwdkmpr

    Try shorting the unused inputs to common.

  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2016

    Created by: bcarlton

    It looks like a negative number (top bit set - '8 ').

  • adccommunitymod (AutomationDirect)

    Created Date: September 08,2016

    Created by: steveola

    Thank you for the suggestions, guys. It magically fixed itself, no wiring changes. I 've used this ladder a few times, I have no idea what happened.

    Steve

  • adccommunitymod (AutomationDirect)

    Created Date: September 08,2016

    Created by: kewakl

    Thank you for the suggestions, guys. It magically fixed itself, no wiring changes. I 've used this ladder a few times, I have no idea what happened.

    Steve

    Just keep in mind

    kewakl's first maxim : any problem that magically fixes itself, will magically unfix itself!

    kewakl's first maxim's first corollary : at the most inopportune time

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 08,2016

    Created by: steveola

    The odd part is I 've used this ladder in six other instruments. One of which I put in my luggage and flew to a spit of land in the middle of the ocean call "Mauritius " where it is still running.

    AD makes some good stuff.

    (Though if I ever get my hands around the neck of the guy that decided on the clip mechanism for the 05/06 cards . . .) :)