adccommunitymod (AutomationDirect) asked a question.
Created Date: February 19,2013
Created By: JoeMcFerron
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hi, I have an H2-EBC100 and am communicating with F2-8AD4DA-2 analog modules via Modbus-TCP. I can read and write the inputs and outputs just fine. But I'm having trouble setting the input and output ranges, formats, and bit-widths. I 've attached the manual for the module. It mentions EBC100 a few times, but mostly refer to D2-250 (and other) PLCs. So I believe I may be encountering a memory translation error. The manual lists 'V-memory ' locations (I'm not sure what the 'V ' refers to), but when I look up those addresses in the HoldingRegister they are blank. Any ideas? Thanks. -Joe
Created Date: February 19,2013
Created by: franji1
this question was also asked on the Host Engineering forum and was answered there
http://forum.hosteng.com/index.php/topic,1064.0.html
Created Date: February 19,2013
Created by: JoeMcFerron
Hi,
I have an H2-EBC100 and am communicating with F2-8AD4DA-2 analog modules via Modbus-TCP. I can read and write the inputs and outputs just fine. But I'm having trouble setting the input and output ranges, formats, and bit-widths.
I 've attached the manual for the module. It mentions EBC100 a few times, but mostly refer to D2-250 (and other) PLCs. So I believe I may be encountering a memory translation error. The manual lists 'V-memory ' locations (I'm not sure what the 'V ' refers to), but when I look up those addresses in the HoldingRegister they are blank.
Any ideas? Thanks.
-Joe