adccommunitymod (AutomationDirect) asked a question.
Created Date: October 27,2011
Created By: bob1371
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello, Working on a program for a height cutter and trying to make things easier for operator. Currently a cut height is entered ie. 28.500 " and a part is cut. It is then measured ie. 28.433 and the operator does the math and hopefully adds .067 " to original cut height (28.500 + .067 = 28.567) and enters the new value. I want to allow them to enter the cut height, run a test part and measure, then enter the new measured height. Let the plc do all the math for them. I need to do this out to 3 decimal places. 1. Can this work? 2. Can someone point me in the right direction? system is a DL450 plc. In the program it appears it's using the "print " command to send a value to the parker servo drive that runs the actuator. HMI is a Cmore. Thanks for any help or info. Bob
Created Date: October 27,2011
Created by: Bob S BN
1. Can this work?
2. Can someone point me in the right direction?
1, yes, I'm sure it can be done.
2, You'll need to add another "numeric entry " button to the c-more to enter the offset value. Perhaps an "add offset " and "subtract offset " discrete buttons as well.
In PLC add a rung;
if (positive differential contact) "add offset " button push is on, LDD "cut length " memory location, ADDD "offset value " memory location, OUTD "cut length " memory location.
This will add the offset value to the "cut length memory location. Make another rung like it to SUBD to decrease the cut length.
This is a down and dirty method, but hopefully will get you started.
Created Date: October 27,2011
Created by: bob1371
Hello,
Working on a program for a height cutter and trying to make things easier for operator.
Currently a cut height is entered ie. 28.500 " and a part is cut. It is then measured ie. 28.433 and the operator does the math and hopefully adds .067 " to original cut height (28.500 + .067 = 28.567) and enters the new value.
I want to allow them to enter the cut height, run a test part and measure, then enter the new measured height. Let the plc do all the math for them. I need to do this out to 3 decimal places.
1. Can this work?
2. Can someone point me in the right direction?
system is a DL450 plc. In the program it appears it's using the "print " command to send a value to the parker servo drive that runs the actuator.
HMI is a Cmore.
Thanks for any help or info.
Bob