adccommunitymod (AutomationDirect) asked a question.
Created Date: August 16,2010
Created By: dieseltwitch
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I'm having problems keeping a connection to a dl05, I'm using the AD USB to 232 adaptor. I can keep a connection for about 2 minutes, them it dies.... Any ideas? I'm using a Mac book, running windows 7 in a virtual machine. It's worked fine for a year now. I did have this plc setup to do field io out of the secondary com port. And had to play with the com setting a bit to get that to work. Could that have done something to it? Please help
Created Date: August 20,2010
Created by: stimpsonjcat
Can't see the 2nd port affecting the first.
what happens on the RX/TX lights when the comm fails?
Created Date: August 16,2010
Created by: dieseltwitch
I'm having problems keeping a connection to a dl05, I'm using the AD USB to 232 adaptor. I can keep a connection for about 2 minutes, them it dies.... Any ideas?
I'm using a Mac book, running windows 7 in a virtual machine. It's worked fine for a year now. I did have this plc setup to do field io out of the secondary com port. And had to play with the com setting a bit to get that to work. Could that have done something to it?
Please help