adccommunitymod (AutomationDirect) asked a question.
DL-105 Power Failure
Created Date: December 27,2014
Created By: aabeck
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have a DL-105 & with good 120 power at the input, but the PLC does not power up. I have opened it up hoping to find a blown fuse, but don't see one. Is there a fuse on-board, or do I have to start testing electronic components to find the outage?:(
Created Date: December 27,2014
Created by: bcarlton
Please provide the model number of the DL-105 (F1-130xxxxx)
Created Date: December 28,2014
Created by: aabeck
It's a F1-130DR, 85-264VAC power, 10DC in, 8 relay out, with 24VDC - 5 amp supply output.
Created Date: December 28,2014
Created by: Tinker
I have a DL-105 & with good 120 power at the input, but the PLC does not power up.
I have opened it up hoping to find a blown fuse, but don't see one.
Is there a fuse on-board, or do I have to start testing electronic components to find the outage?:(
You do realize there are "no user serviceable parts inside " right?
That said, I suspect R1 is a "fusible resistor ", I just checked a working 105 and R1 was 10 ohms, you might check yours, but if it is open, there has to be a reason why. I just took a look at a printed DL105 manual I have, no schematic of the power supply of course, not even a block diagram. However, the copyright on the manual is 1996, suggesting the DL105 design is around 20 years old. No doubt some upgrades have been done over the years, but I think you may have some difficulty finding single unit quantities of some of the old parts.
Since you have relay outputs you can't be using any high speed output functions, how about "high " speed input? if not, personally I'd transcribe the program to a CLICK, if that is not an option, then I'd recommend just buying a new 105.
I understand the desire to repair the thing, in fact I'm on my way to put a new '06 in machine to replace one with bad relays. Once I have the old one out, I will pry it apart, and if I can find relays, I will solder new ones in, and keep the ting for a spare, but I did buy a new PLC first to keep the machine running.
Created Date: December 28,2014
Created by: aabeck
You do realize there are "no user serviceable parts inside " right?
Yes, but fixing unfixable things is a hobby of mine, also, this PLC is out of a stripped machine I was hoping to get working for toying with (I mean practicing with) at home - never actually used a 105 on a machine I built.
Created Date: December 28,2014
Created by: aabeck
Tinker,
I just checked R1, of the 8 connections, a few were 0 ohms to each other & others were infinite. On yours, what were the readings per connection?
Created Date: December 29,2014
Created by: Tinker
Tinker,
I just checked R1, of the 8 connections, a few were 0 ohms to each other & others were infinite. On yours, what were the readings per connection?
Well, like I said, there have no doubt been some updates over the years (or my dyslexia struck again) On the unit I looked at R1 (At least I think it was marked R1, in any case, the first component the Line terminal trace connects to) is a two axial lead cylindrical device that looks like a wire wound resistor (and no doubt that is what it is, with a "flame proof " outer coating allowing it to be used as a fuse, I only mentioned it because you were looking for a fuse)
With only two leads, there was only one pair of points to measure and I got 10ohms.
An 8 lead resistor would be a resistor array and perhaps relatively unlikely to be part of the power supply, certainly not on the high voltage side.
Created Date: December 29,2014
Created by: aabeck
On mine, R1 is a strip on the side board under the relays, like it is a bank of 4 or 7 (with a common) resistors. Don't see any wire wound's in this one.
Created Date: December 29,2014
Created by: plcnut
A high resolution photo of the front and back of the board would be great.
Created Date: January 01,2015
Created by: aabeck
Pics are attached. Don't worry about the 4 white wires going off to the left, I replaced the bridge rectifier, trying that with no luck.
Unfortunately, the main board is partially blocked by the side boards.
Created Date: January 13,2015
Created by: aabeck
Doesn't anyone from Automation Direct monitor these forums & provide answers?