adccommunitymod (AutomationDirect) asked a question.

PLC Type Not Supported

Created Date: June 25,2014

Created By: david222

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have just purchased Dsoft5 software. Trying to get a program out of a 06 PLC for validation purposes. I have the communication settings from the manufacturer that built the machine. When I try to connect I get "PLC type (03800002) is not supported by any installed knowledge base " When IT installed the software they did a complete install, not custom. Any help?? Thanks David


  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2014

    Created by: Bob S BN

    Which port are you trying to connect to?

    The 15 pin secondary can be software programmed for many different protocals.

    The small port has fixed settings that should connect for programming and is typically used for that purpose.

  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2014

    Created by: scott.lawrence

    also, what DS version?

    and what controller make & firmware? I know OP said an 06, but which one?

  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2014

    Created by: jwbaker3

    On the DS Launch window go to the Applications tab and the PLC's supported will be in the center window.

    JW

  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2014

    Created by: david222

    Thanks for all of the suggestions. I spoke with tech support and they are telling me that I did not get a good software install.

    Thanks Again.

    David

  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2014

    Created by: david222

    I have just purchased Dsoft5 software. Trying to get a program out of a 06 PLC for validation purposes. I have the communication settings from the manufacturer that built the machine. When I try to connect I get "PLC type (03800002) is not supported by any installed knowledge base " When IT installed the software they did a complete install, not custom. Any help??

    Thanks

    David

    Expand Post