adccommunitymod (AutomationDirect) asked a question.

Programming GS1 Drive to automatically go to desired settings after pressing run

Created Date: January 22,2018

Created By: carsont

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

How do I program my GS1 Drive to go to a desired frequency after pressing run? I don't want to have to set the frequency/RPM manually using the potentiometer nor up/down keys after pressing run. I am using the GS1 drive to control a motor for a positive-displacement pump. Should I disable Line Start Lockout (P6.30)? Or do I need to use an analog input and change the source of operation for the frequency command in order to do this?


  • adccommunitymod (AutomationDirect)

    Created Date: January 22,2018

    Created by: carsont

    How do I program my GS1 Drive to go to a desired frequency after pressing run? I don't want to have to set the frequency/RPM manually using the potentiometer nor up/down keys after pressing run. I am using the GS1 drive to control a motor for a positive-displacement pump. Should I disable Line Start Lockout (P6.30)? Or do I need to use an analog input and change the source of operation for the frequency command in order to do this?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 23,2018

    Created by: g.mccormick

    you could wire one of the DIs then setup that DI to be apreset speed. (Atleast maybe, if the GS1 allows the preset speed inputs)