Internal Database Security Advisory
SA-00022

Advisory ID
SA-00022
CVSS Score
7.5
Title
C-More EA9 Improper Path Traversal
Description
EXECUTIVE SUMMARY
CVSS v3 7.5
ATTENTION: Exploitable remotely/low attack complexity
Vendor: AutomationDirect
Equipment: C-MORE EA9 HMI
Vulnerabilities: Path Traversal, Stack-Based Buffer Overflow, Plaintext Storage of a Password

2. RISK EVALUATION
Successful exploitation of these vulnerabilities could allow an attacker to exploit a remote device and inject malicious code on the panel.

3. TECHNICAL DETAILS
3.1 AFFECTED PRODUCTS
The following versions of C-MORE EA9 HMI, a display system used for interfacing with controllers, are affected:

C-MORE EA9 HMI EA9-T6CL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T7CL: Version 6.77 and prior
C-MORE EA9 HMI EA0-T7CL-R: Version 6.77 and prior
C-MORE EA9 HMI EA9-T8CL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T10CL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T10WCL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T12CL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T15CL: Version 6.77 and prior
C-MORE EA9 HMI EA9-T15CL-R: Version 6.77 and prior
C-MORE EA9 HMI EA9-RHMI: Version 6.77 and prior
C-MORE EA9 HMI EA9-PGMSW: Version 6.77 and prior
3.2 Vulnerability Overview
3.2.1 Improper Limitation of a Pathname to a Restricted Directory ('Path Traversal') CWE-22
There is a function in Automation-Direct C-MORE EA9 HMI that allows an attacker to send a relative path in the URL without proper sanitizing of the content.

CVE-2024-25136 has been assigned to this vulnerability. A CVSS v3.1 base score of 7.5 has been calculated; the CVSS vector string is (AV:N/AC:L/PR:N/UI:N/S:U/C:N/I:N/A:H)

CVE-2024-25136 has been assigned to this vulnerability. A CVSS v4 base score of 8.7 has been calculated; the CVSS vector string is (AV:N/AC:L/AT:N/PR:N/UI:N/VC:H/VI:N/VA:N/SC:N/SI:N/SA:N).

3.3 BACKGROUND
CRITICAL INFRASTRUCTURE SECTORS: Commercial Facilities, Critical Manufacturing, Energy, Water and Wastewater
COUNTRIES/AREAS DEPLOYED: Worldwide
COMPANY HEADQUARTERS LOCATION: United States

3.4 RESEARCHER
Tomer Goldschmidt of Claroty Research - Team82 reported these vulnerabilities to CISA.

4. MITIGATIONS
AutomationDirect recommends that users update C-MORE EA9 HMI to V6.78. https://www.automationdirect.com/support/software-downloads

CISA recommends users take defensive measures to minimize the risk of exploitation of these vulnerabilities, such as:

Minimize network exposure for all control system devices and/or systems, ensuring they are not accessible from the internet.
Locate control system networks and remote devices behind firewalls and isolating them from business networks.
When remote access is required, use more secure methods, such as Virtual Private Networks (VPNs), recognizing VPNs may have vulnerabilities and should be updated to the most current version available. Also recognize VPN is only as secure as the connected devices.
CISA reminds organizations to perform proper impact analysis and risk assessment prior to deploying defensive measures.

CISA also provides a section for control systems security recommended practices on the ICS webpage on cisa.gov/ics. Several CISA products detailing cyber defense best practices are available for reading and download, including Improving Industrial Control Systems Cybersecurity with Defense-in-Depth Strategies.

CISA encourages organizations to implement recommended cybersecurity strategies for proactive defense of ICS assets.

Additional mitigation guidance and recommended practices are publicly available on the ICS webpage at cisa.gov/ics in the technical information paper, ICS-TIP-12-146-01B--Targeted Cyber Intrusion Detection and Mitigation Strategies.

Organizations observing suspected malicious activity should follow established internal procedures and report findings to CISA for tracking and correlation against other incidents.

No known public exploitation specifically targeting these vulnerabilities has been reported to CISA at this time.

5. UPDATE HISTORY
March 26, 2024: Initial Publication
Products
C-More EA9 HMI
Version
V1.0
Initial Date
3/26/2024
Current version date
3/26/2024
Created By
, 3/26/2024 10:51 AM
Last Modified By
, 1/31/2025 3:30 PM