Internal Database Security Advisory
SA-00016

Advisory ID
SA-00016
CVSS Score
9.8
Title
CLICK PLC CPU Modules C0-1x CPUs Authentication Bypass
Description
1. EXECUTIVE SUMMARY'

CVSS v3 9.8

ATTENTION: Exploitable remotely/low attack complexity

Vendor: Automation Direct

Equipment: CLICK PLC CPU modules

Vulnerabilities: Authentication Bypass Using an Alternate Path or Channel, Cleartext Transmission of Sensitive Information, Unprotected Storage of Credentials

2. RISK EVALUATION
Successful exploitation of these vulnerabilities could allow an attacker to log in as a currently or previously authenticated user or discover passwords for valid users.

3. TECHNICAL DETAILS
3.1 AFFECTED PRODUCTS
Automation Direct reports these vulnerabilities affect the following CLICK PLC CPU modules:

CLICK PLC CPU Modules: C0-1x CPUs with All firmware prior to v3.00

3.2 VULNERABILITY OVERVIEW


3.2.2 AUTHENTICATION BYPASS USING AN ALTERNATE PATH OR CHANNEL CWE-288
All programming connections receive the same unlocked privileges, which can result in a privilege escalation. During the time the PLC is unlocked by an authorized user, an attacker can connect to the PLC and read the project without authorization.

CVE-2021-32984 has been assigned to this vulnerability. A CVSS v3 base score of 9.8 has been calculated; the CVSS vector string is (AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H).

3.3 BACKGROUND
CRITICAL INFRASTRUCTURE SECTORS: Commercial Facilities, Critical Manufacturing, Information Technology
COUNTRIES/AREAS DEPLOYED: Worldwide
COMPANY HEADQUARTERS LOCATION: United States
3.4 RESEARCHER
Irfan Ahmed and Adeen Ayub of Virginia Commonwealth University and Hyunguk Yoo of the University of New Orleans reported these vulnerabilities to Automation Direct.

4. MITIGATIONS
Automation Direct reports these vulnerabilities are all mitigated by Version 3.00 and recommends users update software and firmware to the latest version.

Automation Direct also recommends users follow its security guidelines.

CISA recommends users take defensive measures to minimize the risk of exploitation of these vulnerabilities. Specifically, users should:

Minimize network exposure for all control system devices and/or systems, and ensure that they are not accessible from the Internet.
Locate control system networks and remote devices behind firewalls, and isolate them from the business network.
When remote access is required, use secure methods, such as Virtual Private Networks (VPNs), recognizing VPNs may have vulnerabilities and should be updated to the most current version available. Also recognize VPN is only as secure as its connected devices.
CISA reminds organizations to perform proper impact analysis and risk assessment prior to deploying defensive measures.

CISA also provides a section for control systems security recommended practices on the ICS webpage on us-cert.cisa.gov. Several recommended practices are available for reading and download, including Improving Industrial Control Systems Cybersecurity with Defense-in-Depth Strategies.

Additional mitigation guidance and recommended practices are publicly available on the ICS webpage on us-cert.cisa.gov in the Technical Information Paper, ICS-TIP-12-146-01B--Targeted Cyber Intrusion Detection and Mitigation Strategies.

Organizations observing any suspected malicious activity should follow their established internal procedures and report their findings to CISA for tracking and correlation against other incidents.

No known public exploits specifically target these vulnerabilities.

This product is provided subject to this Notification and this Privacy & Use policy.

Vendor
Automation Direct
Products
CLICK PLC CPU Modules C0-1x CPUs
Version
V1.0
Initial Date
Current version date
6/15/2021
Created By
, 11/14/2023 6:55 PM
Last Modified By
, 11/14/2023 6:55 PM